:SYSTem:SOFTware:LICenses:BORRow?
Instrument:
N1010A
DCA-X
DCA-M
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:SYSTem:SOFTware:LICenses:BORRow? <package license> <number of days>
Where <package license> specifies the package license using the string listed in the following Software License Package Arguments table.
Where <number of days> is an integer that specifies how many days you wish to borrow the license. The valid range of days is 1 to 90.
Query Response
Boolean, 1 or 0
Description
Use this query to borrow a software license package from Keysight's Pathwave License Manager. You must specify both the package license and the number of days that you wish to use (borrow) the license. The query returns a '1' if the license was successfully borrowed and a '0' if the borrow failed.
Package | Query Argument |
---|---|
Research and Development Package | L-RND |
Manufacturing Package | L-MFG |
Signal Integrity Package | L-SNT |
N1002014A 14 Port Switch License Package | L-SW17 |
N1002048A 48 Port Switch License Package | L-SW48 |
N1002128A 128 Port Switch License Package | L-128 |
Requires FlexDCA revision A.06.80 and above.
Example
:SYSTem:SOFTware:LICenses:BORRow? "L-SNT" 90