:WAVeform:STATus?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:STATus?
Description
Queries the status of the waveform data and returns the strings shown in the following table. Use the :REASon child query to return a string that indicates why the data is invalid or questionable. For example, "INV" is returned when the TDR Peeling signal-processing function is used and the TDR reference plane is positioned off screen.
| Response | Description |
|---|---|
| CORR | The waveform data is correct. |
| INV | The waveform data is invalid. |
| QUES | The waveform data is questionable. |
Query the data using one of the following commands:
- :WAVeform:YFORmat:ASCii:YDATa?
- :WAVeform:YFORmat:DOUBle:YDATa?
- :WAVeform:YFORmat:FLOat:YDATa?
- :WAVeform:YFORmat:WORD:YDATa?
- :WAVeform:XYFORmat:ASCii:YDATa?
- :WAVeform:XYFORmat:ASCii:XDATa?
- :WAVeform:XYFORmat:DOUBle:YDATa?
- :WAVeform:XYFORmat:DOUBle:XDATa?
- :WAVeform:XYFORmat:FLOat:YDATa?
- :WAVeform:XYFORmat:FLOat:XDATa?
Requires FlexDCA revision A.03.00 and above.