:WAVeform:XYFormat:ASCii:YDATa?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:XYFormat:ASCii:YDATa?
Description
Returns the y-axis data in ASCII for XY-formatted data as ASCII comma-separated values. The data is sent in linear format starting from the graticule's left side and progressing to the right side. Use the :WAVeform:XYFormat:ASCii:XDATa? query to return the x-axis data. Use the :WAVeform:XYFormat:POINts? query to return the number of points contained in the array. The XY-format data format is designed for waveforms that have been sampled using unequal time separations between adjacent data points. Unequal time separations occurs with pattern waveforms or when using a precision timebase.