Common Commands
86100D Legacy Command | Similar FlexDCA Command |
---|---|
*CLS | *CLS |
*ESE | *ESE |
*ESR? | *ESR? |
*IDN? | *IDN? |
*LRN? | :DISK:SETUP:SAVE
The instrument setup data is saved to a file rather than returned to the controller. |
*OPC | *OPC |
*OPT? | *OPT? |
*RCL | :DISK:SETUP:RECall
The instrument setup data is recalled from a file rather than a register. Instrument setups are not saved to registers in FlexDCA. |
*RST | *RST or :SYSTem:DEFault |
*SAV | :DISK:SETUP:SAVE
The instrument setup data is saved to a file rather than saved to a register. Instrument setups are not saved to registers in FlexDCA. |
*SRE | *SRE |
*STB? | *STB? |
*TRG | *TRG |
*TST? | *TST? |
*WAI | *WAI |