:DISK:SETup:RECall
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:DISK:SETup:RECall "filename"
Description
Loads a state setup file into FlexDCA. Use the :DISK:SETup:SAVe command to save a state setup file. Setup files use the .setx file extension and by default are saved in the %USER_DATA_DIR%\Setups folder.
C:\Users\user\Documents\Keysight\FlexDCA\Setups
The hardware (extended module) configuration settings are always saved with a state file. When opening an state setup file, use the :SETup:RECall:HCONfig command to select whether to import the extended module configuration settings.
To assign the loading of an instrument setup file to the Multi-Purpose button, use the :SYSTem:MPButton:FUNCtion command.