Acquisition Setup (Jitter Mode)
This topic describes the Acquisition Setup dialog's Waveform tab when FlexDCA is in Jitter Mode. Use the Acquisition Setup dialog's Waveform tab to define the way you want the instrument to acquire data from the input waveform. In Jitter Mode, normally all dialog settings are grayed out and FlexDCA automatically configures the settings including setting the Samples / UI to Automatic. However, in certain conditions FlexDCA will allow you to manually set the Samples / UI. For example, this can happen if you are using a signal processing operator like SIRC. It is recommended that you use the Automatic setting.