ADS Dataset (.ds)
Meas. mode:
Eye
Scope
Waveform type:
NRZ
PAM4
Pulse
Keysight ADS Files (.ds)
Keysight Advanced Design System (ADS) files (*.ds) can be saved in both Oscilloscope and Eye/Mask modes. Files saved in this format can be used for simulations within Keysight’s Advanced Design System software. In a typical use case, the waveform would be specified as the source for a VtDataset
(Time-domain voltage source) component. The following figure shows a simple ADS example that performs transient analysis using a VtDataset
as a source: