Pattern Waveform (.wfmx)

Instrument
N1000A
N109x
Flex Apps:
FlexDCA

Internal Format Pattern Waveform Files (.wfmx)

Pattern waveform files (.wfmx) can be saved in both Oscilloscope and Eye/Mask modes. The instrument must be pattern locked to save pattern waveforms. Pattern waveforms are long, single-valued waveforms that span multiple UIs, up to the entire pattern length. The pattern waveform ASCII files (.csv) includes a header followed by amplitude (y) values for each data point. Click File > Save > Waveform to open the Waveform Save dialog from which you can save a pattern waveform.

Settings for Saving Pattern Format Files
✔ Pattern Lock
✔ Acquire Entire Pattern
⚫ Wrap Waveform (Eye Mode)
✔ = selected. ✘ = unselected. ⚫ = don't care

The following limits apply to saving pattern waveforms:

  • Up to 4096 points can be saved for each UI.
  • Pattern lengths up to 2 23 can be saved.

Because of the large number of UIs and high resolution (points-per-symbol) possible, pattern waveforms may require a large amount of memory. Since pattern waveforms are saved in ASCII files, you can import then into spreadsheet, math, and text editing applications. Pattern waveforms can also be imported back into color gray-scale memory as an eye diagram. If you plan on loading a pattern waveform back into the instrument, be sure to also save the instrument setup. You will need to load (restore) the instrument settings at the same time that you load the associated pattern waveform.

The ability to save pattern waveforms requires the following features:

  • Eye/Mask or Oscilloscope instrument mode with pattern lock triggering.
  • At least one channel or function (invert, subtract, or magnify) turned on.

Option N1010A-201, Advanced Waveform Analysis License, is not required in order to save pattern waveforms.

Options for saving Pattern Waveforms (.csv format)

Select Convert Holes and Clipped values to specify that missing or clipped data points be converted to amplitude values:

  • Missing data (holes) can occur under certain conditions.
  • If an amplitude value is greater than the current settings allow, the clipped value is listed as the string "Infinity". Converted clipped values will be set to the maximum posible value (positive or negative).

Select Limit to to write all waveform values at the specified number of significant digits. The default number of significant digits is 6.

The following table shows the last header lines with the first few data points in a Pattern Waveform (.csv) file. In the file, fields are separated with carriage return/line feeds. The name and value pairs are separated with commas. In this example, the maximum waveform value before clipping is 9.3249E−4 Watts. A marker placed on this data point in FlexDCA would show NaN (Not a Number). In the Unconverted Data file, notice that clipped values are expressed as Infinity, but in the Converted Data file these same values are set to the amplitude value at the screen's maximum graticule level. Notice also that all amplitude values have been rounded at 6 significant digits, which is the default Limit to setting.

Example of Data Point Conversion in .CSV File
Unconverted Data in File Converted Data in File
…
…
Pattern Length, 127
X Units, Second
Y Units, Watt
Data, 
Infinity
Infinity
0.000324403129719199
-1.14260479488511E-05
-1.92323921718938E-06
5.35599942609364E-06
1.23683709516537E-06
8.92236134171939E-07
0.000511116740339243
Infinity
Infinity
…
…
Pattern Length, 127
X Units, Second
Y Units, Watt
Data, 
9.32490E-4
9.32490E-4
3.24403E-4
-1.14260E-5
-1.92324E-6
5.35600E-6
1.23684E-6
8.92236E-7
5.11117E-4
9.32490E-4
9.32490E-4

File types for NRZ and PAM4

Starting with FlexDCA version A.05.60, pattern waveforms can be saved for PAM4 waveforms in addition to NRZ waveforms. The resulting csv files have the minor differences as shown in red in the following table.

Examples of Differences Between CSV File Header for NRZ and PAM4 Signals
NRZ Signal PAM Signal
File Format, WaveformPattern
Format Version, 1
Instrument, N1010A
SwVersion, P.05.60.248
SerialNumber, 
Date, 12/21/2016 07:46:46 GMT-08:00
Source Name, Channel 1A

Points, 1015
Signal Type, NRZ
Channel Bandwidth, 1.5E+10
Channel Noise, 5.2E-05
XOrg, 8.74537237933125E-12
XInc, 1.25710472034706E-11
Bit Rate (b/s), 9953280000
Points/Bit, 7.99212598425197
Pattern Length, 127
X Units, Second
Y Units, Volt
Data, 
…
…
File Format, WaveformPattern
Format Version, 2
Instrument, N1010A
SwVersion, P.05.60.248
SerialNumber, 
Date, 12/21/2016 07:45:01 GMT-08:00
Source Name, Channel 1A

Points, 1015
Signal Type, PAM4
Channel Bandwidth, 1.5E+10
Channel Noise, 5.2E-05
XOrg, 9.56596135863221E-12
XInc, 1.25710472034706E-11
Symbol Rate (Baud), 9953280000
Samples/UI, 7.99212598425197
Pattern Length, 127
X Units, Second
Y Units, Volt
Data, 
…
…

To save a pattern waveform

  1. Establish a pattern lock.
  2. Click Setup > Acquisition Setup.
  3. In the Acquisition Setup dialog's Waveform tab, select Acquire Entire Pattern.
  4. Close the dialog.
  5. Click File > Save > Save Waveform.
  6. In the Files of Type drop-down list, select Pattern Waveform (*.csv) or Waveform Files (Internal) (*.wfmx).
  7. Click Save.

Saving pattern waveforms is slower when an N1060A-PTB's precision timebase is active. For faster saves, turn off the precision timebase.

Patterns that include a large number of UIs and high resolution involve large amounts of data. Saving these files may require several hours and one or two gigabytes (GB) of memory.

If you plan on loading a saved pattern waveform back into the instrument, be sure to also save the instrument setup. You will need to load (restore) the instrument settings at the same time that you load the associated pattern waveform.

To load a pattern waveform into waveform memory

  1. Click File > Waveform Memory. Pattern waveform files have the file extension .csv or .wfmx.
  2. Select the Memory tab.
  3. Click Load From File.
  4. In the Files of Type drop-down list, select Pattern Waveform (*.csv) or Waveform Files (Internal) (*.wfmx).
  5. Select the file and click Open.
  6. In the Waveform Memories dialog, click the Display On/Off button to display the waveform.

More Information