Run SCPI Script

Instrument
N1000A
Flex Apps:
FlexDCA

SCPI Scripts

To configure the button to run SCPI scripts. Four default scripts are loaded, one for each of FlexDCA's modes. To expand the dialog so that you can add your custom scripts, in the dialog under Multi-Purpose Function select Run SCPI Script as shown in the following picture.

SCPI scripts are recordings of your front-panel key presses translated into equivalent programming commands. Scripts allow you to automate the setup of complex instrument configurations and settings.

When Use Single Script for All Modes is selected, the MultiPurpose button will run a single script regardless of the current instrument mode. This script does not exist, so you must create the script, give it any name that you want, and place it in the \Scripts user folder. This folder has a sub-folder named \Multi-Purpose Button. You cannot save scripts to this folder as it is a shortcut to a folder that is write protected.

When Use Single Script for All Modes is cleared, a unique script can be selected to run in each instrument mode (Oscilloscope, Eye/Mask, Jitter, and TDR/TDT). There are default mode scripts located in the \Scripts\Multi-Purpose Button folder as shown in the following table. You can create and assign your own scripts for each mode. Click Browse to select the script which should be placed in the \Scripts user folder.

Default Scripts for Each FlexDCA Mode
Instrument Mode Use Single Script
for All Modes
Setting
Default Script in \Multi-Purpose Button folder
On Off
Oscilloscope Modes ♦ MultiPurpose Default Scope Mode.scpi
Eye/Mask Modes ♦ MultiPurpose Default Eye Mode.scpi
Jitter Modes ♦ MultiPurpose Default Jitter Mode.scpi
TDR/TDT Modes ♦ MultiPurpose Default TDR Mode.scpi

A Default Setup does not clear or reset the currently assigned SCPI script. To reset the dialog to the default scripts, click Setup > Factory Preset.

Oscilloscope Mode Default Script

Prerequisite

Oscilloscope mode is running with at least one waveform displayed.

Action

Several measurements are made.

Script

// MultiPurpose Default Scope Mode.scpi
:MEASure:OSCilloscope:RISetime
:MEASure:OSCilloscope:FALLtime
:MEASure:OSCilloscope:PERiod
:MEASure:OSCilloscope:JITTer
:MEASure:OSCilloscope:VAMPlitude

Eye/Mask Mode Default Script

Prerequisite

Eye/Mask mode is running with at least one waveform displayed.

Action

Several measurements are made.

Script

// MultiPurpose Default Eye Mode.scpi
:MEASure:EYE:RISetime
:MEASure:EYE:FALLtime
:MEASure:EYE:JITTer
:MEASure:EYE:AMPLitude
:MEASure:EYE:BITRate
:MEASure:EYE:CROSsing

Jitter Mode Default Script

Prerequisite

Jitter mode is running with at least one waveform displayed.

Action

Several measurements are made.

Script

// MultiPurpose Default Jitter Mode.scpi
:MEASure:JITTer:DDPWs
:MEASure:JITTer:FOVer2
:MEASure:JITTer:JN:SJN J2
:MEASure:JITTer:JN
:MEASure:JITTer:JN:SJN J9
:MEASure:JITTer:JN

TDR/TDT Mode Default Script

Prerequisite

TDR/TDT mode is running with a TDR module. A DUT is setup with channel 1A as the stimulus source.

Action

A TDR measurement is made with a time-domain response waveform shown in Ohms and another time-domain response waveform shown in volts. Three measurements are performed, with two of the measurements made over waveform regions. Finally, a tracking marker is turned on.

Script

// MultiPurpose Default TDR Mode.scpi
:TDR:STIMulus:CHAN1A:STEP ON
:TRACe1:COLor TCOLor1
:TRACe1:DUT DUT1
:TRACe1:PARameter T1_1
:TRACe1:OPERator OHMS
:TRACe1:CWINdow TOHMs1
:TRACe1:DISPlay ON
:TRACe2:COLor TCOLor1
:TRACe2:DUT DUT1
:TRACe2:PARameter T1_1
:TRACe2:OPERator VOLTs
:TRACe2:CWINdow TVOLts1
:TRACe2:DISPlay ON
:TIMebase:SCALe 2.0000E-10
:TIMebase:POSition 0
:MEASure:REGions:COUNt 2
:MEASure:REGions:STATe ON
:MEASure:REGions:REGion1:X1 2.0000E-10
:MEASure:REGions:REGion1:X2 4.0000E-10
:MEASure:REGions:REGion2:X1 5.0000E-10
:MEASure:REGions:REGion2:X2 7.0000E-10
:MEASure:OSCilloscope:VAMPlitude:SOURce1 TRACe2
:MEASure:TDR:VAVerage:REGion REGion1
:MEASure:TDR:VAVerage
:MEASure:TDR:VMINimum:REGion REGion2
:MEASure:TDR:VMINimum
:MARKer:Y1A:SOURce TRACe2
:MARKer:Y1A:STATe TRACk