Factory Preset
Click Setup > Factory Preset to restore FlexDCA to its factory preset settings. Factory preset is the combination of the default settings and the settings listed in the following table.
| Feature | Setting |
|---|---|
| Miscellaneous Settings | |
| List of recent setup files | Cleared |
| List of recent DCA-X hosts | Cleared |
| Use Compact Signals Palette | Off |
| Show Marker Tools on Screen | On |
| Multi-Purpose button | Removes any configuration settings |
| Display Setup dialog Settings (Appearance Tab) | |
| UI Theme | Tungsten |
| Show Animations | on |
| Dialog Size | Normal |
| Mode Switch Animation | No Animation |
| Overlap Display Tabs | off |
| Use On-Screen Keyboard | off |
| Connection Setup Dialog Settings | |
| On Connect Setting | Restore |
| Connection Type to DCA-X | LAN |
| SICL Interface | gpib0 |
| GPIB Address | 7 |
| SCPI Server Setup | |
| GPIB | Enabled |
| VXI-11 | Enabled |
| USB | Enabled |
| Telnet | Disabled |
| Sockets | Enabled |
| USB | Enabled |