Time Measurement Toolbar

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ

With the exception of the jitter measurements, Oscilloscope time measurements are designed for single-valued waveforms. When a jitter measurement is selected, the instrument's measurement database is enabled. Jitter is the only oscilloscope measurement that uses the database as a source. The waveform data that is sampled is accumulated in the measurement database. In order to view this data, you must select the color grade (or gray scale) display persistence mode.

Scope Time Measurements and Supported Waveforms
MeasurementWaveform Types
NRZPAM4PAM6PAM8
Delta Time● ● ● ●
Duty Cycle● ● ● ●
Fall Time● ● ● ●
Frequency● ● ● ●
Jitter●
Pulse Width (Negative)● ● ● ●
Period● ● ● ●
Phase● ● ● ●
Pulse Width (Positive)● ● ● ●
Rise Time● ● ● ●
Time at Max● ● ● ●
Time at Min● ● ● ●
Time at Amplitude● ● ● ●
Time at Edge● ● ● ●