Time at Amplitude

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ

Time at Amplitude is the measure of the time at which the specified edge amplitude occurs on the displayed waveform.

When this measurement is selected, a dialog appears from which you select the edge number, direction, amplitude value, and if it is restricted to a measurement region.

This measurement may be compatible with PAM4 signals, depending on the PAM4 waveform. PAM measurement capability requires the Research and Developement or Manufacturing package license.

Configurable Measurement Parameters

This measurement is affected by the following settings (click Measure > Configure Base Measurements):

To measure

  1. Click the button and enter the waveform edge number, amplitude, and direction at which to perform the measurement.
  2. If measurement regions are enabled, select the area over which the measurement is to be performed: a Region or the Entire Display.

SCPI Command

:MEASure:OSCilloscope:TVOLt