Negative Pulse Width

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

The Oscilloscope mode — Pulse Width is defined as the time from the middle threshold of the first falling edge to the middle threshold of the next rising edge. The measurement can be restricted to a measurement region. These points are marked by two waveform annotation labels. The lower and upper threshold levels do not directly affect the negative pulse width measurement. However, the lower and upper threshold levels are used to determine whether or not a waveform edge is valid for the measurement.

This measurement is designed for single valued waveforms in oscilloscope mode only.

This measurement is not compatible with PAM4 signals.

Configurable Measurement Parameters

This measurement is affected by the following settings (click Measure > Configure Base Measurements):

To measure

  1. Select Oscilloscope Mode.
  2. Click the toolbar's Time tab.
  3. Click the toolbar's More buttons to locate the – Pulse Width button.
  4. Click the button.
  5. If measurement regions are enabled, the Select Measurement Region, Setting dialog is displayed. Select the area over which the measurement is to be performed: a Region or the Entire Display.

SCPI Command

:MEASure:OSCilloscope:NWIDth