Amplitude Measurement Toolbar

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
Scope Amplitude Measurements and Supported Waveforms
Measurement Waveform Types
NRZ PAM4 PAM6 PAM8
Amplitude at Lower ● ● ● ●
Amplitude at Middle ● ● ● ●
Amplitude at Time ● ● ● ●
Amplitude at Upper ● ● ● ●
Amplitude ● ● ● ●
Average ●
Average Power ● ● ● ●
Maximum ● ● ● ●
Minimum ● ● ● ●
Optical Modulation Amplitude ● ● ● ●
Overshoot ● ● ● ●
Peak-Peak Amplitude ● ● ● ●
Peak-Peak at Hit Ratio ● ● ● ●
Preshoot ● ● ● ●
RMS ● ● ● ●
Waveform Base ● ● ● ●
Waveform Top ● ● ● ●