<Script> Element

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Use this element to specify the Matlab or Python script to run. A path is required if the script is located in a folder other than the default \User Measurements folder. The script can be based on any of the following file types that you create:

  • MATLAB scripts (*.m)
  • MATLAB Standalone Application (*.exe)
  • Python scripts (*.py)

Do not use spaces or hyphens when selecting a filename for your script.

Parent Elements

<Function>

Child Elements

None

Attributes

Example

  • <Function>
  • …
  • <Script>EyeMeasurement.m</Script>
  • …
  • </Function>