<String> Element

Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

The <String> element adds a User-Defined Control to the User Operator Setup dialog. The control is a blank string-entry field, unless you include the optional <Default> element which allows you to pre-populate the string. The string can be up to 128 characters. Escape characters are not allowed. In order for your script to access this setting, the "Name" attribute in the parent <Control> element must be the name of a script string variable.

  • <Control Name = "Text">
  • <String>
  • <Default>Enter the DUT ID here!</Default>
  • </String>
  • </Control>

Parent Elements

Child Elements

Attributes

None

Example

  • <Function>
  • …
  • <Control Name = "Text">
  • <String>
  • <Default>Enter the DUT ID here!</Default>
  • </String>
  • …
  • </Function>