Time at Min
The Time at Min is a measure of the time at which the first data sample with the minimum waveform level first occurs. The measurement can be restricted to a measurement region. Time at Min is position independent. Therefore, the instrument uses the entire waveform on the display graticule to determine the minimum signal level. An annotation label is placed at the result.

In TDR/TDT mode, the measurement can be performed on any waveform that is displayed in one of the following content windows:
- Waveform
- Time-Ohms
- Time-Volts
- Time-%
Configurable Measurement Parameters
This measurement is not affected by setting in the Configure Base Measurements dialog.
To measure
- Click the button.
- If measurement regions are enabled, the Select Measurement Region, Setting dialog is displayed. Select the area over which the measurement is to be performed: a Region or the Entire Display.
SCPI Command
:MEASure:TDR:TMINimum