Time at Edge

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter

The Time at Edge is the measure of the time at which the specified waveform edge occurs on the displayed waveform. When this measurement is selected, a dialog appears from which you select the edge number, direction, threshold value, and if it is restricted to a measurement region.

In TDR/TDT mode, the measurement can be performed on any waveform that is displayed in one of the following content windows:

  • Waveform
  • Time-Ohms
  • Time-Volts
  • Time-%

Configurable Measurement Parameters

This measurement is affected by the following settings (click Measure > Configure Base Measurements):

To measure

  1. Click the button and select the waveform edge number, threshold, and direction at which to perform the measurement.
  2. If measurement regions are enabled, select the area over which the measurement is to be performed: a Region or the Entire Display.

SCPI Command

:MEASure:TDR:TEDGe