:CALibrate:MODule
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:CALibrate:MODule {ENABled | DISabled | PARTial}, "<DCA-M-name>"
Where <DCA-M-name> is the N109x-series DCA module's name that is shown on the DCA-M block on the Hardware Diagram. For example, "N1092B-US12345678".
Query Syntax
:CALibrate:MODule? "<DCA-M-name>"
Description
Enables or disables module calibrations for the indicated module.
- ENABled
-
Selects all module calibrations for the module to be performed. - DISabled
-
Prevents all module calibrations for the module from being performed. - PARTial
-
Indicates that some module calibrations are enabled and some are disabled.
To perform the module calibration, use open the FlexDCA application and send the :CALibrate:MODule:STARt command to the DCA-M.
Example Command
:CALibrate:MODule ENABled, "N1092A-US12341678"