:CALibrate:MODule:STATus:DTEMperature?

Flex Apps:
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram

Query Syntax

:CALibrate:MODule:STATus:DTEMperature? "<DCA-M-name>"

Where <DCA-M-module-name> is the name that identifies the DCA-M module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1092B-US12345678".

Description

Queries the change in the DCA-M module's temperature (°C) from the time when the last module calibration was performed. If a calibration has not yet been performed, a value of NaA (9.91E+37) is returned. A calibration should be performed if the change in DCA-M temperature exceeds ±5°C.

Example Returned Status

2.340000000E+00