:CALibrate:MODule:STATus:DETails?

Flex Apps:
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram

Query Syntax

:CALibrate:MODule:STATus:DETails? "<DCA-M-name>"

Where <DCA-M-module-name> is the name that identifies the DCA-M module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1092B-US12345678".

Description

Queries a string of status details of an DCA-M module's calibration. The following is an example of a typical returned string:

Time of last Calibration: 10/23/2020 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"

If a calibration is recommended, the following text is placed at the beginning of the above string:

"Requires Clock Recovery Calibration, …"

If a calibration has not yet been performed, the following string is returned:

"This calibration has never been performed in this instrument."

Example Returned Status String

"Elapsed cal time has exceeded 10 hours.,Time of last Calibration: 09/20/2012 15:11:05,Elapsed Calibration Time: 26 days,Temperature Change: 2.58 C"