:CALibrate:MODule:STATus:TIME?

Flex Apps:
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram

Query Syntax

:CALibrate:MODule:STATus:TIME? "<DCA-M-name>"

Where <DCA-M-module-name> is the name that identifies the DCA-M module on the Hardware Diagram. The name is the combination of the <model number>-<serial number>. For example, "N1092B-US12345678".

Description

Queries the date and time when the last DCA-M module's calibration was performed. If a calibration has not yet been performed, an empty string is returned.

Example Returned Status String

"09/20/2012 15:11:05"