:STATus:LOCal:EVENt?

Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations

Query Syntax

:STATus:LOCal:EVENt?

Description

Reads the local event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (LOCAL REG), which indicates if FlexDCA has been placed in local mode (exited remote mode). Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 0 (LCL) of the User Event Register.

Local Register Commands
Register Read Write Command
Event ♦   :STATus:LOCal:EVENt?
Enable (mask) ♦ ♦ :STATus:LOCal:ENABle
Local Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — LOCAL REG
Enable
Register
               
Sets to Bit 0 (LCL) of User Event Register

Bit Definitions

LOCAL REG
A true indicates that FlexOTO has transitioned from remote mode to local mode.