:STATus:OPERation:ENABle

Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
FlexOTO Instance:
Hardware Diagram
Stations

Command Syntax

:STATus:OPERation:ENABle <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

:STATus:OPERation:ENABle?

Description

Use the operation enable register to mask the ability to report bits in the operation event register.

Operation Register Commands
Register Read Write Command
Event ♦   :STATus:OPERation:EVENt?
Enable (mask) ♦ ♦ :STATus:OPERation:ENABle
Operation Status Registers for FlexOTO
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32,768 16,384 8,192 4,096 2,048 1,024 512 256 128 64 32 16 8 4 2 1
Event
Register
— CAL InstReady — — — ACQ — CLCK — — — — — — —
Enable
Register
                               
Sets to Bit 7 (OPER) of Status Byte Register

Bit Definitions

ACQ
A true indicates that an enabled bit in the acquisition event status register has been set and that the data acquisition has satisfied the specified completion criteria.
CAL
A true indicates that an enabled bit in the calibration event status register has been set by a calibration completing.
CLCK
A true indicates that an enabled bit in the clock recovery event status register has been set.
InstReady
A true indicates that an enabled bit in the instrument event status register has been set. This occurs when FlexOTO pauses Test Program execution to allow a user measurement to be made.