:STATus:TRIGger:ENABle

Flex Apps:
FlexDCA
FlexRT
FlexPLL

Command Syntax

:STATus:TRIGger:ENABle <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

:STATus:TRIGger:ENABle?

Description

Enters a decimal-weighted value in the trigger enable register that masks the ability to report bits in the trigger event register.

Trigger Register Commands
Register Read Write Command
Event ♦   :STATus:TRIGger:EVENt?
Enable (mask) ♦ ♦ :STATus:TRIGger:ENABle
Trigger Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — TRG
Enable
Register
               
Sets to Bit 0 (TRG) of Status Byte Register

Bit Definitions

TRG
A true indicates that a trigger has been received.