:STATus:TRIGger:EVENt?

Flex Apps:
FlexDCA
FlexRT
FlexPLL

Query Syntax

:STATus:TRIGger:EVENt?

Description

Reads the trigger event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (TRG), which indicates if a trigger has been received. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 0 (TRG) of the Status Byte Register. The TRG event register stays set until it is cleared by reading the register or using the *CLS (clear status) command. If your application needs to detect multiple triggers, clear the trigger event register after each trigger. If you are using the Service Request to interrupt a computer operation when the trigger bit is set, you must clear the event register after each time it is set.

Trigger Register Commands
Register Read Write Command
Event ♦   :STATus:TRIGger:EVENt?
Enable (mask) ♦ ♦ :STATus:TRIGger:ENABle
Trigger Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — — — — — TRG
Enable
Register
               
Sets to Bit 0 (TRG) of Status Byte Register

Bit Definitions

TRG
A true indicates that a trigger has been received.