:STATus:CRECovery:EVENt?

Flex Apps:
FlexDCA
FlexRT
FlexPLL

Query Syntax

:STATus:CRECovery:EVENt?

Description

Reads the clock recovery event register to determine the status of individual status bits. The decimal-weighted value of the register is returned.

Clock Recovery Register Commands
Register Read Write Command
Event ♦   :STATus:CRECovery:EVENt?
Enable (mask) ♦ ♦ :STATus:CRECovery:ENABle
Clock Recovery Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— LKFIN LKSTRT — — — LOCK UNLK
Enable
Register
               
Sets to Bit 7 (CLCK) of Operation Status Register

Bit Definitions

UNLK
True indicates that clock recovery is unlocked. This occurs when an or N1060A Precision Waveform Analyzer module becomes unlocked or trigger loss has occurred. To determine if the RELock command has completed, use the :CRECovery:LOCKed?.
LOCK
True indicates that clock recovery is locked or a trigger capture has occurred.
LKSTRT
True indicates that the clock recovery re-lock routine has started.
LKFIN
True indicates that the clock recovery re-lock routine has finished.