:STATus:CRECovery:ENABle

Flex Apps:
FlexDCA
FlexRT
FlexPLL

Command Syntax

:STATus:CRECovery:ENABle <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

:STATus:CRECovery:ENABle?

Description

Enters a decimal-weighted value in the clock recovery enable register that masks the ability to report bits in the clock recovery event register.

Clock Recovery Register Commands
Register Read Write Command
Event ♦   :STATus:CRECovery:EVENt?
Enable (mask) ♦ ♦ :STATus:CRECovery:ENABle
Clock Recovery Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— LKFIN LKSTRT — — — LOCK UNLK
Enable
Register
               
Sets to Bit 7 (CLCK) of Operation Status Register

Bit Definitions

UNLK
True indicates that clock recovery is unlocked. This occurs when an or an N1060A Precision Waveform Analyzer module becomes unlocked or trigger loss has occurred. To determine if the RELock command has completed, use the :CRECovery:LOCKed?.
LOCK
True indicates that clock recovery is locked or a trigger capture has occurred.
LKSTRT
True indicates that the clock recovery re-lock routine has started.
LKFIN
True indicates that the clock recovery re-lock routine has finished.