:STATus:USER:EVENt?

Flex Apps:
FlexDCA
FlexRT
FlexPLL

Query Syntax

:STATus:USER:EVENt?

Description

Reads the user event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used is bit 0 (LCL), which indicates if FlexPLL has been placed in local mode (exited remote mode). The other 15 bits are reserved. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically OR'ed, which results in setting true bit 1 (USR) of the Status Byte Register.

User Register Commands
Register Read Write Command
Event ♦   :STATus:USER:EVENt?
Enable (mask) ♦ ♦ :STATus:USER:ENABle
User Status Registers
Bit 7 6 5 4 3 2 1 0
Bit
Weight
128 64 32 16 8 4 2 1
Event
Register
— — — SLOT4 SLOT2 SLOT3 SLOT1 LCL
Enable
Register
               
Sets to Bit 1 (USR) of Status Byte Register

Bit Definitions

LCL
A true indicates that FlexPLL has transitioned from remote mode to local mode. This status bit originates from the local event register.
SLOT1
Reserved for future use.
SLOT3
Reserved for future use.
SLOT2
Reserved for future use.
SLOT4
Reserved for future use.