IHislipInstr::Address
Description
Returns the device's TCP/IP address.
VB Prototype
Dim value As String
value = object.Address
C++ Prototype
HRESULT get_Address(
BSTR* Address
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview