IHislipInstr::DeviceName
Description
Returns the LAN device name.
VB Prototype
Dim value As String
                                            value = object.DeviceName
                                        
C++ Prototype
HRESULT get_DeviceName(
                                        
  BSTR* DeviceName
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview