IHislipInstr::HostName
Description
Returns the TCP/IP hostname of the device. If no host name is available, this attribute returns an empty string.
VB Prototype
Dim value As String
                                            value = object.HostName
                                        
C++ Prototype
HRESULT get_HostName(
                                        
  BSTR* HostName
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview