IHislipInstr::ProtocolVersion
Description
Returns the negotiated HiSLIP protocol version.
VB Prototype
Dim value As Long
                                            value = object.ProtocolVersion
                                        
C++ Prototype
HRESULT get_ProtocolVersion(
                                        
  long* ProtocolVersion
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview