IHislipInstr::ProgID
Description
Returns the programmatic ID that can be used by COM to create this object.
VB Prototype
Dim value As String
value = object.ProgID
C++ Prototype
HRESULT get_ProgID(
BSTR* ProgID
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview