IHislipInstr::ControlREN

Description

Controls the state of the REN line and, optionally, the remote/local state of the device. This operation asserts or de-asserts the REN line according to the specified mode. 

VB Prototype

ControlREN(
  mode As RENControlConst
)

C++ Prototype

HRESULT ControlREN(
  RENControlConst mode
);

Parameters

mode

Specifies the state of the REN line and, optionally, the device remote/local state.

Return Value

Refer to the table of return codes.

See Also

 Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview