IHislipInstr::ResourceName
Description
Returns the VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resource string used to open/init the resource.
VB Prototype
Dim value As String
value = object.ResourceName
C++ Prototype
HRESULT get_ResourceName(
BSTR* ResourceName
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview