IHislipInstr::OverlapEnabled
Description
Returns or sets the HiSLIP overlap enabled mode.
VB Prototype
Dim value As Boolean
                                            value = object.OverlapEnabled
                                        
object.OverlapEnabled = value 
                                        
C++ Prototype
HRESULT get_OverlapEnabled(
                                        
  VARIANT_BOOL* OverlapEnabled
);
		
HRESULT put_OverlapEnabled(
                                        
  VARIANT_BOOL OverlapEnabled
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview