IHislipInstr::Timeout
Description
Returns or sets the I/O timeout, in milliseconds, for I/O communication on this resource session.
VB Prototype
Dim value As Long
                                            value = object.Timeout
                                        
object.Timeout = value 
                                        
C++ Prototype
HRESULT get_Timeout(
                                        
  long* Timeout
);
		
HRESULT put_Timeout(
                                        
  long Timeout
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview