IHislipInstr::SoftwareManufacturerName
Description
Returns the name of the manufacturer of this software component.
VB Prototype
Dim value As String
                                            value = object.SoftwareManufacturerName
                                        
C++ Prototype
HRESULT get_SoftwareManufacturerName(
                                        
  BSTR* SoftwareManufacturerName
);
Return Value
Refer to the table of return codes.
See Also
Address, Close, ComponentVersion, ControlREN, DeviceName, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, HostName, Init, LastStatus, LockRsrc, LockState, MaxMessage, OptionString, OverlapEnabled, ProgID, ProtocolVersion, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, SpecVersion, Timeout, UnlockRsrc, IHislipInstr Overview