Sync Search Length (RFID)
1 mSec (See RFID Standard Setups/Presets Table)
0 to
The text box sets the sync search measurement interval in seconds. (Since it is difficult to specify measurement interval using Bits or Tari when PIE is selected in ASK mode, the units are in seconds.)
The text box becomes active when is set to .
It generally does not make sense to do a sync search over the entire acquired time data because a typical RFID signal typically contains multiple bursts with potentially different modulation formats.
When is off, the parameter specifies where to start the sync search (offset from the start of the acquired data) and the parameter specifies the length of the sync search.
See Also