Acquisition Length (RFID)
: 10 mSec (See RFID Standard Setups/Presets Table)
The parameter specifies the signal acquisition length in seconds. affects the and parameters.
When is on, the is the same as , and the determines the measurement region.
See Also