:CHANnel:EYE:CWINdow

Command Syntax

:CHANnelN:EYE:CWINdow TIME{1:4}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:EYE:CWINdow?

Description

The :CHANnel{N}:EYE:CWINdow command lets you assign a real-time eye waveform to a Waveform content window.

Command Arguments and Content Windows
Argument Displayed Waveform
Content Window
Number of
Available Windows
Scale Units
Programmatically Via
Front Panel
TIME{1:4} Waveform 4 4 Y-Axis: Volts or Watts (linear scale)
X-Axis: seconds