:CHANnel:EYE:XPOSition

Command Syntax

:CHANnelN:EYE:XPOSition <time>
            

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<time> is a double.

Query Syntax

:CHANnelN:EYE:XPOSition?

Description

Sets the channel N horizontal time position (center display location) of the real-time eye display.

This command directly affects the real-time eye's horizontal position setting in UI (unit interval) units (see the :CHANnel:EYE:UIXPosition command).

To set the horizontal time scale of the real-time eye display in seconds-per-division, use the :CHANnel:EYE:XSCale command.