:CHANnel:EYE:UUNits
Command Syntax
:CHANnelN:EYE:UUNits {UINTerval | SECond}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:EYE:UUNits?
Query Response
{UINT | SEC}
Description
This command specifies the user interface's units option for the real-time eye horizontal Scale and Position controls. You can select either Unit Intervals (UIs) or time (in seconds).
To specify the real-time eye horizontal scale and position in terms of UI units, use the :CHANnel:EYE:UIXRange and :CHANnel:EYE:UIXPosition commands.
To specify the real-time eye horizontal scale and position in terms of time units, use the :CHANnel:EYE:XSCale and :CHANnel:EYE:XPOSition commands.