:CHANnel:EYE:WINDow:TRACking

Command Syntax

:CHANnelN:EYE:WINDow:TRACking  {{ON | 1} | {OFF | 0}}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:EYE:WINDow:TRACking?

Query Response

{1 | 0}

Description

Specifies whether a signal tracks the global eye window definition or uses its own eye window definition.

The global eye window definition is set using the :MEASure:EYE:WINDow commands (see Eye Window Configuration Commands).

Example Command Sequence

:CHANnel2:EYE:WINDow:TRACking OFF
:CHANnel2:EYE:WINDow:METHod EOPening
:CHANnel2:EYE:WINDow:LEFT 40.0
:CHANnel2:EYE:WINDow:RIGHt 60.0