:CHANnel:EYE:XSCale
Command Syntax
:CHANnelN:EYE:XSCale <seconds_per_div>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<seconds_per_div> is a double.
Query Syntax
:CHANnelN:EYE:XSCale?
Description
Sets the channel N horizontal time scale of the real-time eye display in seconds-per-division.
This command directly affects the real-time eye's horizontal range setting in UI (unit interval) units (see the :CHANnel:EYE:UIXRange command).
To set the horizontal position (center display location), use the :CHANnel:EYE:XPOSition command.
Only the center UI is valid for the recovered clock edge. You can display up to 10 UIs to show context before and after the center UI.