:CHANnel:EYE:UIXRange

Command Syntax

:CHANnelN:EYE:UIXRange <time_in_UI>
            

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<time_in_UI> is a double in UI (unit interval) units.

Query Syntax

:CHANnelN:EYE:UIXRange?

Description

Sets the channel N horizontal time range (width) of the real-time eye display in UI units.

This command directly affects the real-time eye's horizontal time/div setting in seconds (see the :CHANnel:EYE:XSCale command).

To set the horizontal position (center display location) of the real-time eye display in UI units, use the :CHANnel:EYE:UIXPosition command.

Only the center UI is valid for the recovered clock edge. You can display up to 10 UIs to show context before and after the center UI.