:CHANnel:EYE:WINDow:METHod
Command Syntax
:CHANnelN:EYE:WINDow:METHod {EOPening | CLOCk}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:EYE:WINDow:METHod?
Description
This command specifies how the eye window used for measurements is determined:
-
EOPening— Measures within an eye window defined by left and right opening locations.Use the
:CHANnel:EYE:WINDow:LEFTand:CHANnel:EYE:WINDow:RIGHtcommands to specify the left and right opening location values. The default values are 40% (left) and 60% (right) which identifies the central 20% of symbol period. -
CLOCk— Measures within an eye window that is a width percentage at the location of the recovered clock edge.Use the
:CHANnel:EYE:WINDow:WIDThcommand to specify the width percentage value.
This command is equivalent to the settings in the Eye tab of the Configure Measurements dialog box.