:CHANnel:EYE:WINDow:WIDTh
Command Syntax
:CHANnelN:EYE:WINDow:WIDTh<percent>
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
<percent> is a double.
Query Syntax
:CHANnelN:EYE:WINDow:WIDTh?
Description
When the "At Clock Time" eye window determination method is selected (see :CHANnel:EYE:WINDow:METHod), this command specifies the UI percentage width about the recovered clock location to use as the eye window. A zero percent for this setting means only the recovered clock location is used.
This command is equivalent to the settings in the Eye tab of the Configure Measurements dialog box.