:CHANnel:SNDRatio:FILE:NAME

Command Syntax

:CHANnelN:SNDRatio:FILE:NAME "filename"

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:SNDRatio:FILE:NAME?

Query Response

"string"

Description

When FILE is selected as the SNDR standard (see :CHANnel:SNDRatio:STANdard), this command specifies the name of the SNDR standard definition file.

Use the :CHANnel:SNDRatio:FILE:RELoad command to reload the SNDR standard definition file, for example, after loading a setup file that has FILE selected as the SNDR standard.